Skip to main content
1-844-731-7989
KOHLER Generators Logo

Search

House at storm

Be ready before the next storm arrives

2026 Hurricane Preparedness & Backup Power

Get Your Free Quote

Call (844) 731-7989 or fill out the form.

Hurricane preparedness is vital for homeowners across the United States. This is especially true as the Atlantic hurricane season brings stronger, less predictable weather.

Warm waters fuel hurricanes that develop across the Atlantic basin. These systems can quickly intensify, producing dangerous wind speeds, heavy rainfall, and destructive storm surge.

During National Hurricane Preparedness Week, the message remains consistent: start preparing before forecasters even predict a storm.

Find a dealer

Lightning strike in the sky, houses, purple sky

Why Hurricane Preparedness Matters

As storms grow stronger in mid-August and on, steady rain and rising winds can damage power lines and vital power systems.

Without preparation, outages can quickly lead to:

  • Food spoilage within hours

  • Unsafe indoor temperatures

  • Loss of communication

  • Increased safety risks for families and pets

Hurricane preparedness is about reducing these risks before they happen, not reacting once conditions worsen in real time.

The risks of waiting until a storm is happening

When hurricanes are already developing, demand for generators and services increases rapidly. Homeowners often rely on real time updates from the National Hurricane Center, but by that point, options are limited.

Delaying hurricane preparedness can result in:

  • Limited generator inventory

  • Longer installation timelines

  • Reduced access to certified installers

  • Increased stress during emergency conditions

  • Panic buying replaces strategic planning

Preparing before hurricane season ensures your home is protected without the pressure of an approaching storm.

Backup power when it matters most

Immediate power during outages

During hurricanes, outages can happen suddenly as wind speeds increase and infrastructure is impacted. A standby generator ensures a seamless transition to backup power.

Your home continues running essential systems, including:

  • HVAC systems for temperature control

  • Refrigeration to preserve food

  • Lighting and critical appliances

  • Medical devices and equipment

This level of performance is especially important during extended outages caused by major storms.

Woman touching screen
People at front door at a rainy day

Safety and security

Hurricane preparedness includes protecting your home from unnecessary risk. A standby generator eliminates many of the safety concerns associated with temporary solutions.

With a permanent system:

  • No refueling is required during severe weather

  • No extension cords create hazards

  • Power is distributed safely throughout your home

  • Security systems and alarms remain active

This helps maintain safety even as conditions outside become more severe.

Your Home Your Comfort

Maintaining comfort during a hurricane supports stability and well-being.

Backup power allows you to:

  • Keep indoor temperatures consistent

  • Continue working remotely

  • Stay connected through charged devices

  • Maintain daily routines

  • Even as storms intensify across the Atlantic basin, your home remains functional.

Professional working on generator

Protect your home from damage

Power outages can lead to long-term damage if systems fail. Flooding, humidity, and mechanical shutdowns can create costly issues.

A standby generator helps:

  • Keep sump pumps running to prevent flooding

  • Reduce mold and moisture buildup

  • Protect plumbing systems from damage

  • Preserve food and essential supplies

These protections extend beyond the storm and help reduce recovery time.

Install before peak hurricane season

Timing is critical in hurricane preparedness. Installing a standby generator involves multiple steps that require planning and coordination.

Typical installation includes:

  • In-home consultation and system sizing

  • Permitting and approvals

  • Professional installation and testing

As hurricane season progresses, especially around mid-August, demand increases significantly.

Installing early helps:

  • Avoid seasonal delays

  • Ensure full product availability

  • Secure installation before peak demand

  • Allow time to test and understand your system

Preparation ahead of time ensures your home is ready before storms develop.

Professional working on generator

Ongoing service supports reliability

Routine maintenance is a key part of hurricane preparedness. A generator must be ready to perform when needed.

Service typically includes:

  • Full system inspection

  • Oil and filter replacement

  • Battery testing

  • Performance diagnostics

  • Regular maintenance helps ensure your system performs reliably during a power outage.

Build a complete hurricane preparedness plan

A standby generator is one part of a broader strategy.

Additional steps include:

A comprehensive approach helps ensure your home and family are fully prepared.

Prepare now, before the next storm

Hurricane preparedness is about acting early.

Installing a standby generator now provides:

  • Reliable backup power during outages

  • Increased safety and protection

  • Greater comfort

  • Confidence throughout hurricane season

Schedule your Consultation

Take the next step in hurricane preparedness today.

Find a dealer

KOHLER Generators Logo

© 2026 Discovery Energy, LLC dba Rehlko. All Rights Reserved