Protect your Houston home with backup power.
Free 10-Year Extended Warranty & $300 Rebate* with generator purchase. Limited time offer June 3–July 15, 2026.
Get Your Free Quote
Call (844) 731-7989 or fill out the form.
Whole Home Generators Built for Houston Storms
Houston weather changes fast and outages can hit without warning. That is why homeowners trust KOHLER standby generators for automatic backup power in seconds.
Keep essentials running including AC, refrigerator, security, and lights through storms and outages. Built in the USA, engineered for extreme winds, and supported by Houston area dealers, KOHLER delivers reliable power when it matters most.


How to buy a whole home generator
Contact us via phone or complete the free quote form
Get connected to a local certified KOHLER dealer
Receive a no-obligation quote for generator installation
Have your new generator installed by your dealer
Still have questions?
The total cost of a standby home generator depends on several factors, including:
Generator size and power capacity
Whole-home vs essential-circuit coverage
Natural gas or propane setup
Electrical and gas line work
Permits and site preparation
Installation complexity
Because every home is different, most homeowners schedule a free site evaluation to receive a custom recommendation and quote. A certified dealer can assess your home’s power needs and installation requirements before providing pricing.
Most standby generator installations are completed within a few days once equipment and permits are ready. The overall process can take longer depending on:
Permit approvals
Utility coordination
Generator availability
Weather and site conditions
Gas or electrical upgrades
Yes. Financing is commonly available through many authorized dealers.
Will the generator automatically start if I’m not home? Yes. A standby generator is specifically designed to start automatically even if you are away from home. When utility power is lost, the generator’s automatic transfer switch (ATS) detects the outage, signals the generator to start, and transfers your home’s electrical load to backup power — typically within about 10 seconds. Once utility power returns, the system automatically switches back and shuts the generator down.

How a home generator works
Your generator is connected to your home’s electrical systems, continuously monitoring the utility power.
Your generator’s Automatic Transfer Switch (ATS) detects the disruption in utility power within seconds.
The generator supplies your home with electricity until your utility power is restored.
As power is restored, the ATS automatically switches back to utility grid power. Your generator remains in standby until the next outage.
Talk to a real person
Call 844-844-1732 to speak with a helpful Kohler professional. Hours of operation: Mon-Fri 7AM-7PM CST
Terms & Conditions:
*Limited time offer. Offer is available to customers who order a qualifying KOHLER residential generator** between June 3 and July 15, 2026, through a participating U.S.A. or Canada Kohler certified partner (Kohler certified dealer, Kohler certified installer, or Kohler certified wholesaler). This offer applies to the generator only. To qualify for this offer, a Kohler certified partner must submit the required online submission form and valid proof of order (consumer quote or invoice) by June 15, 2026. The generator must be installed and registered no later than September 30, 2026, by a Kohler certified partner. Offer not available at eCommerce or retail businesses, except Kohler certified dealers participating in Home Depot or Lowe’s retail installation programs. Kohler resellers are not eligible for this offer. Offer may not be combined with other offers or promotions. Generators registered by a non-certified Kohler partner or the homeowner are not eligible for extended warranties. Generators used in an off-grid/prime power application are not eligible for extended warranties. Void where prohibited. Offer valid on new generator sales only. The manufacturer has the right to cancel or modify this offer at any time without notice. **Valid Products: KOHLER 10RESV(L), 12RES, 12RESV(L), 14RCA(L), 20RCA(L), 24RCLA, 26RCA(L), 30RCLA, 38RCLC, 48RCLC, 60RCLB generators. Please allow four to eight weeks from submission date to receive your free 10-year extended warranty.