Skip to main content
1-844-731-7989
KOHLER Generators Logo

Search

How Long Can a Standby Generator Run Continuously?

TLDR

  • Standby generators can run for several days or longer. Those connected to a natural gas line can remain operational throughout an outage.

  • Runtime depends on fuel supply, how many appliances you're running, and whether the generator is properly maintained.

  • Unlike portable generators, standby generators are permanently connected to a fuel source, so they don't need manual refueling to keep running.

  • During extended outages from storms or grid failures, a continuously running standby generator keeps heating, cooling, refrigeration, and lighting all online.

Key Takeaways:

  • Standby generators can run for several days or longer with fuel, and natural gas systems may run continuously during outages.

  • Generator runtime ultimately depends on fuel supply, load, and maintenance. They’re designed for extended operation, but they do need some monitoring.

  • Continuous generator runtime helps maintain essential home systems.

How long can a standby generator run continuously? In most cases, home standby generators are designed to run for extended periods, often several days, as long as they have a continuous fuel supply and are properly maintained.

Unlike portable generators, standby generators are permanently installed and connected to a fuel source, like natural gas or propane. This allows them to operate much longer without manual refueling, and in many cases, generators connected to a natural gas line can run continuously throughout an outage.

What Affects Generator Runtime?

There are a few key factors that determine how long a generator can safely run:

  • Fuel supply: Natural gas systems can run indefinitely, while propane systems depend on tank size.

  • Load demand: Running more appliances with your generator increases fuel consumption and strains the system.

  • Maintenance: Oil levels, filters, and cooling systems need to be in good condition for continuous operation.

  • Weather conditions: Extreme heat or cold can affect generator performance and efficiency.

Most modern standby generators are built for continuous operation, but they still require routine monitoring. Some generator systems include automatic shut-offs or alerts if maintenance is needed, and regular servicing ensures the generator can handle extended outages without interruption.

Extended outages caused by storms or grid failures can last for days, and a standby generator that runs continuously helps maintain heating, cooling, refrigeration, lighting, and other essential systems. For homeowners, this means greater comfort and peace of mind during long power outages.

Find a KOHLER Home Generators dealer near you to stay one step ahead.

KOHLER Generators Logo

© 2026 Discovery Energy, LLC dba Rehlko. All Rights Reserved