Skip to main content
1-844-731-7989
KOHLER Generators Logo

Search

A large brick house with a Kohler generator along a wall in a residential neighborhood at night with a storm and lightning outside and the lights on inside Generators 101

How a Home Generator Can Help Save You Money

Key Takeaways:

  • Prevent Costly Damage: Backup power protects against flooding, burst pipes, and mold during outages.

  • Avoid Hotel & Grocery Costs: Stay home safely and keep food fresh with reliable generator power.

  • Boost Property Value: A permanently installed generator adds resale appeal and long-term value.

  • Lower Insurance Rates: Generators reduce risk of damage, potentially qualifying your home for lower premiums.

  • Smart Budget Protection: Avoid unexpected expenses and maintain comfort during severe weather.

Are you starting the new year with smarter spending habits and a budget in mind? Unexpected power outages could derail your plans. With a Kohler home generator designed for reliable, whole-home power, you can avoid drains on your finances that may come with an outage.

Reliable power helps you avoid expensive property repairs.

Ensuring your home’s systems function properly during an outage helps protect your home from costly damages. For a 2,500-square foot home, sump pump failure resulting in a two-inch flood has an estimated cost of $26,500 to restore. According to the Insurance Information Institute, burst or frozen pipes caused by lack of heat and water use could cost around $12,500 to repair. With water comes mold, an unwelcome problem that can cost anywhere between $500–$30,000 to address.

You can stay at home during an outage.

Outages caused by winter storms, excessive heat, or hurricanes may make remaining at home unsafe for you and your family. Without power behind your home’s HVAC system, indoor conditions will likely become uncomfortable quickly as temperatures shift. Plus, a lack of lighting could make it difficult to uncover any resulting storm damage that may prove hazardous. While neighbors may need to seek shelter elsewhere during extended outages (racking up potentially expensive hotel fees), backup power from your generator means you and your loved ones can stay put.

Save on replacement groceries.

When an outage occurs, frozen or refrigerated food spoils quickly. Refrigerated food only lasts up to four hours after the power fails—and only if the fridge door remains shut the entirety of that time. A full freezer can keep food safe for up to 48 hours; that number decreases to 24 hours if the freezer is only half full. Ultimately, a power outage could result in replacing spoiled produce, meat, and all other perishable food items in your refrigerator and freezer. Generator power behind your refrigerator and freezer means you can consume food and water safely while you wait out the outage.

Your property value may be higher.

You aren’t the only one with safety in mind—potential buyers also think about protecting their home and family from the effects of power outages. Today’s buyers are increasingly seeking homes with smart upgrades that make their lives easier, like solar panel systems and backup power solutions. As standby generators are permanently installed on your property, your generator is an investment that not only saves you money and stress while you live in your home, but also increases your home’s resale value, especially when you understand the key generator buying factors that influence performance and long term benefits.

Home insurance rates may be lower.

Power that keeps your home’s systems running as they should means you’re less likely to experience damage as a result of system failure. Insurance companies are likely to provide a lower rate on a home that is properly secured from theft, flooding, or other issues that may come in the wake of severe weather or extended outage, especially when backup power is installed and serviced by a local KOHLER dealer. Your generator keeps the lights on, your security system powered, and your sump pump performing—giving you and your insurance company peace of mind.

A man and a woman enjoying themselves at a restaurant as they tap their drink glasses together.

You can’t put a price on peace of mind.

Interested in the potential savings—and stress-free outage experiences—reliable backup power can offer you? Request your free quote today to talk to a dealer about financing options and available generator models.

Need help with your Kohler home generator?

Call Kohler Home Generator Support: 1-833-393-6650 Hours: Monday – Friday, 8:00am to 4:30pm (CT)

woman answering a call for owner support
KOHLER Generators Logo

© 2026 Discovery Energy, LLC dba Rehlko. All Rights Reserved