Skip to main content
1-844-731-7989
KOHLER Generators Logo

Search

Professional working on a generator with cablesInstallation & Maintenance

How Often Should You Service a Home Generator?

Key Takeaways

  • Most standby generators should receive professional service at least once per year, even if they haven’t been used during an outage.

  • A proper generator maintenance schedule typically includes oil changes, inspections, diagnostics, and load testing.

  • Routine home generator maintenance helps ensure reliable startup, longer equipment lifespan, and reduced risk of unexpected failures.

  • Following manufacturer-recommended service intervals helps maintain safe operation and warranty protection.

A standby generator is designed to deliver dependable backup power when outages occur. Whether power is lost during severe storms, grid failures, or extreme weather, homeowners rely on their generator to start automatically and keep essential systems running.

However, like any engine-powered system, generators require routine care to perform reliably over time.

Following a consistent generator maintenance schedule helps ensure:

  • Reliable startup during outages

  • Longer engine and system lifespan

  • Reduced risk of unexpected performance issues

  • Continued warranty compliance

Preventive maintenance isn’t just a recommendation—it’s a key part of protecting your investment in backup power.

Homeowners considering a new standby system can explore available home generators, where you can compare systems designed to provide automatic whole-home backup power.

Understanding Your Generator Maintenance Schedule

A generator maintenance schedule outlines the inspections, servicing, and testing required to keep a standby generator operating safely and efficiently. Maintenance schedules are typically based on several factors, including:

  • Annual service requirements

  • Total runtime hours

  • Fuel type, such as natural gas or propane

  • Environmental conditions like humidity or extreme temperatures

  • How frequently the generator operates

Most standby generators follow both time-based and usage-based service intervals, meaning maintenance may be recommended annually as well as after a certain number of runtime hours.

These intervals help ensure that key components—such as the engine, battery, alternator, and fuel system—remain ready to operate when an outage occurs.

How Often Should You Service a Home Generator?

While maintenance intervals vary slightly depending on the manufacturer and model, most residential standby generators follow a similar schedule.

Annual Maintenance (Recommended Minimum)

Most homeowners should schedule professional generator service at least once per year.

During an annual maintenance appointment, technicians typically perform:

  • Engine oil and filter replacement

  • Air filter inspection or replacement

  • Spark plug inspection

  • Battery testing

  • Fuel system inspection

  • Electrical connection checks

  • Control panel diagnostics

  • Full operational load testing

Even if your generator hasn’t run during an outage, annual maintenance is still recommended. Systems that remain idle for long periods still require inspections to ensure components remain ready for operation.

Guidance from the Federal Emergency Management Agency (FEMA) also emphasizes that generators used for emergency power require routine servicing—including oil changes, inspections, and operational testing—to maintain reliability during extended outages.

Every 100–200 Hours of Runtime

Generators that run frequently—such as during long outages or in areas with unstable electrical grids—may require additional service based on runtime hours.

Typical maintenance performed during these intervals includes:

  • Oil changes

  • Air filter inspection

  • Engine inspection

  • System performance checks

Monitoring runtime hours helps ensure the generator continues to operate efficiently during extended operation.

Professional working on a generator with tools and wearing helmet
Professional working on generator
Close shot of a generator

What Happens If You Skip Generator Maintenance?

Skipping routine generator maintenance can lead to performance issues that may not become apparent until the system is needed during an outage.

Potential risks include:

  • Delayed or failed generator startup

  • Increased engine wear and reduced lifespan

  • Fuel system issues or clogged filters

  • Reduced electrical output during operation

  • Battery failure or electrical faults

Because standby generators often sit idle for extended periods, preventive maintenance plays an important role in keeping the system reliable. Regular servicing helps ensure your generator performs as expected when it matters most.

Factors That May Affect Your Maintenance Schedule

While annual service is sufficient for many homeowners, certain conditions may require more frequent maintenance.

Examples include:

  • Homes located in coastal or high-humidity environments

  • Regions with extreme hot or cold temperatures

  • Generators that run frequently due to grid instability

  • Homes with large electrical loads or whole-home backup systems

  • Properties exposed to dust, debris, or heavy pollen

A certified service technician can help determine whether your generator requires a more customized maintenance schedule based on your environment and usage.

DIY Maintenance vs. Professional Service

Homeowners can perform a few simple visual checks between professional service visits, but most generator maintenance should be completed by trained technicians.

Basic homeowner checks may include:

  • Ensuring the generator area remains clear of debris or vegetation

  • Monitoring system alerts or status indicators

  • Checking that airflow around the generator enclosure remains unobstructed

  • Listening for unusual sounds during routine self-tests

However, professional service ensures:

  • Accurate diagnostics and system testing

  • Proper oil and filter replacement

  • Safe electrical inspections

  • Compliance with manufacturer warranty requirements

Professional inspections provide added confidence that your backup power system will perform as expected during emergencies.

Stay Ahead with a Consistent Maintenance Schedule

A consistent generator maintenance schedule is one of the most effective ways to protect your backup power system.

By scheduling regular service and following manufacturer-recommended intervals, homeowners can help ensure their generator:

  • Starts automatically during power outages

  • Operates efficiently during extended use

  • Maintains long-term reliability and durability

Preventive maintenance today supports dependable performance tomorrow.

If you’re considering installing a standby generator, you can request a free quote for a KOHLER generator and find the right backup power solution for your home. Already a KOHLER customer? Schedule generator maintenance today.

KOHLER Generators Logo

© 2026 Discovery Energy, LLC dba Rehlko. All Rights Reserved