Skip to main content
1-844-731-7989
KOHLER Generators Logo

Search

Woman in front of a open fridgeStorm Preparedness

Extreme Heat and Power Outages: Why an Emergency Standby Generator Is a Summer Essential

Key Takeaways:

Rising temperatures increase AC use and grid demand while reducing the efficiency of transformers and transmission equipment. As a result, heat waves are a common trigger for power outages.

Losing electricity during extreme heat puts cooling, refrigerated food/medications, medical equipment, communications, and security systems all at risk.

An emergency standby generator automatically restores power within seconds of an outage, keeping your essential systems running.

Extreme heat is one of the biggest challenges homeowners face during the summer months. As temperatures climb, electricity demand increases, placing added strain on the electrical grid and raising the risk of power outages.

Losing electricity during a heat wave is certainly an inconvenience, but the risks go beyond that. Without power, air conditioning stops working, refrigerators begin to warm, medical equipment may go dark, and indoor temperatures can quickly become dangerous. For many homeowners, an emergency standby generator offers peace of mind by automatically restoring power when the electrical grid goes down.

Why Does Extreme Heat Increase the Risk of Power Outages?

When temperatures rise, millions of homes and businesses rely more heavily on air conditioning to stay comfortable. This surge in electricity demand places significant stress on the electrical grid.

At the same time, extreme heat can affect the electrical infrastructure itself. High temperatures can reduce the efficiency of transformers, transmission lines, and other equipment, making it more difficult for utilities to meet demand. Combined with summer thunderstorms, high winds, or equipment failures, these conditions can lead to widespread outages.

Although utilities work to maintain grid reliability, prolonged heat waves can increase the risk of both planned and unplanned power interruptions.

What Are the Risks of Losing Power During a Heat Wave?

Power outages during mild weather are inconvenient. During extreme heat, outages can quickly become a health and safety concern.

Without electricity, homeowners may lose access to:

  • Air conditioning and fans

  • Refrigeration for food and medications

  • Internet and communication devices

  • Medical equipment

  • Security systems

  • Lighting

  • Charging for phones and other essential electronics

Indoor temperatures can rise rapidly, especially in homes with limited ventilation. Young children, older adults, and individuals with chronic health conditions are particularly vulnerable to heat-related illnesses.

For households that depend on electrically powered medical devices, even a short outage can create additional challenges.

What Is an Emergency Standby Generator?

An emergency standby generator is a permanently installed backup power system that automatically restores electricity when utility power is interrupted.

Unlike portable generators, standby generators connect directly to your home's electrical system and fuel supply. When an outage occurs, an automatic transfer switch detects the loss of utility power, starts the generator, and transfers your home's electrical load within seconds. Once utility power is restored, the system safely switches back to the electrical grid and shuts down automatically.

Because the entire process is automatic, homeowners don't need to go outside in dangerous weather or manually connect extension cords.

What Are the Benefits of an Emergency Standby Generator During Summer?

Having a standby generator can come in handy all year long, but it’s especially beneficial as temperatures rise.

Stay Cool and Comfortable

One of the greatest benefits of an emergency standby generator is maintaining air conditioning during an outage.

Keeping your cooling system operating helps maintain safer indoor temperatures and improves comfort while utility crews restore power.

Protect Food and Medications

Extended outages often result in spoiled groceries and temperature-sensitive medications.

Backup power keeps refrigerators and freezers running, helping preserve food and reduce unnecessary waste. It also helps maintain proper storage conditions for medications that require refrigeration.

Support Essential Medical Equipment

Many households rely on electrically powered medical devices, including oxygen concentrators, CPAP machines, mobility equipment, and refrigerated medications.

An emergency standby generator helps ensure these critical devices continue operating when utility power is unavailable.

Keep Your Home Connected

Internet service, mobile device charging, and home office equipment all depend on electricity.

Backup power allows families to stay informed through weather alerts, communicate with loved ones, continue working remotely, and monitor emergency information during extended outages.

Protect Your Home

Electricity powers more than lights and appliances. Depending on your home's setup, outages may interrupt sump pumps, security systems, garage door openers, and well pumps.

Keeping these systems operating helps reduce disruptions and may help prevent additional property damage.

How To Prepare for Summer Power Outages

While no one can predict exactly when an outage will occur, homeowners can prepare before temperatures peak.

Consider taking these steps:

  • Schedule routine maintenance for your standby generator.

  • Verify the generator's automatic self-test is operating properly.

  • Keep the area around the generator free of debris and vegetation.

  • Assemble an emergency supply kit with water, nonperishable food, flashlights, batteries, and medications.

  • Charge mobile devices and backup battery packs before major heat events.

  • Monitor weather forecasts and local utility alerts.

Preparing ahead of time helps ensure your backup power system is ready when it's needed most.

Why Automatic Backup Power Matters

Summer outages often occur unexpectedly, especially during periods of extreme heat or severe thunderstorms.

Because an emergency standby generator automatically restores power, homeowners don't have to rush outside in uncomfortable or hazardous conditions to start it. Instead, the system responds within seconds, allowing essential appliances and home systems to continue operating with minimal interruption.

That automatic response can make a meaningful difference during prolonged outages, particularly for households with young children, older adults, or family members with medical needs.

The Bottom Line: Is an Emergency Standby Generator Worth It?

For many homeowners, an emergency standby generator is a long-term investment in safety, comfort, and convenience.

While every home's power needs are different, backup power provides valuable protection during extreme summer weather by helping maintain cooling systems, refrigeration, communication devices, medical equipment, and other essential household systems.

As heat waves become more frequent and electricity demand continues to rise during the summer months, preparing for power outages is an important part of protecting your home. An emergency standby generator helps ensure your household can continue functioning even when the electrical grid is down. Find a KOHLER Home Generators dealer near you and stay prepared.

FAQs

Why does extreme heat cause power outages?

Extreme heat increases electricity demand as more homes and businesses run air conditioning, straining the grid. At the same time, high temperatures reduce the efficiency of transformers and transmission lines, making it harder for utilities to meet demand and increasing the risk of outages.

How is an emergency standby generator different from a portable generator?

An emergency standby generator is permanently installed and connects directly to your home's electrical system and fuel supply. It uses an automatic transfer switch to detect outages and restore power within seconds, unlike portable generators, which require manual setup and fueling.

How quickly does a standby generator turn on during an outage?

A standby generator typically restores power within seconds of detecting a utility outage. An automatic transfer switch senses the loss of power, starts the generator, and transfers your home's electrical load without any action needed from the homeowner.

What appliances can a standby generator power during a heat wave?

Depending on the system's size, a standby generator can power air conditioning, refrigerators and freezers, medical equipment, internet and communication devices, security systems, sump pumps, and lighting throughout an outage.

Who is most at risk during a summer power outage?

Young children, older adults, and individuals with chronic health conditions face the highest risk during summer power outages, since rising indoor temperatures and loss of medical equipment or refrigerated medications can quickly become dangerous.

KOHLER Generators Logo

© 2026 Discovery Energy, LLC dba Rehlko. All Rights Reserved

Extreme Heat and Power Outages: Why an Emergency Standby Generator Is a Summer Essential | KOHLER Generators