Skip to main content
1-844-731-7989
KOHLER Generators Logo

Search

Palm trees at a beach on a windy dayStorm Preparedness

Do Inland Homeowners Need Generators? What NOAA Says About Inland Hurricanes For 2026

Key Takeaways:

Hurricanes can continue causing dangerous weather long after moving inland. Inland communities frequently experience damaging winds, flooding, tornadoes, and prolonged power outages.

NOAA recommends hurricane preparedness for inland and coastal homeowners alike.

Homes with wells, mature trees, or medical equipment may be especially vulnerable during outages. An emergency standby generator automatically restores power during utility interruptions

When people think about hurricanes, they often picture coastal communities boarding up windows, preparing for storm surge, and evacuating before landfall. While coastal areas typically experience the strongest impacts, hurricanes don't simply disappear after reaching shore. Many storms continue hundreds of miles inland, bringing damaging winds, flooding, tornadoes, and widespread power outages to communities far from the coast.

NOAA's outlook for the 2026 Atlantic hurricane season reminds homeowners that every hurricane season deserves preparation. Although seasonal forecasts may predict below-average, near-normal, or above-average activity, it only takes one storm to cause significant damage. For inland homeowners, understanding the risks associated with an inland hurricane can help determine whether backup power is a worthwhile investment.

What Is an Inland Hurricane?

An inland hurricane refers to the impacts of a tropical storm or hurricane after it moves away from the coastline. Although hurricanes gradually weaken after landfall because they lose access to warm ocean water, they often remain capable of producing dangerous weather well inland.

Communities hundreds of miles from the coast may experience:

Damaging straight-line winds

Flash flooding

Saturated ground that causes trees to fall

Tornadoes developing within hurricane rain bands

Extended utility outages

Many homeowners mistakenly believe they are safe simply because they don't live near the ocean. In reality, inland communities frequently experience some of the longest-lasting impacts after hurricanes move inland.

Can Hurricanes Cause Major Outages Even If They’re Not Category 4?

One of the biggest misconceptions about hurricanes is that only the strongest storms cause significant damage.

Even storms that weaken after landfall can produce conditions that interrupt electrical service for days. Heavy rain softens the ground, making trees easier to uproot during strong wind gusts. Fallen trees are one of the leading causes of downed power lines during tropical systems.

Flooding can also damage substations, restrict access to roadways, and delay repair crews attempting to restore service. Because hurricanes often affect multiple counties or even several states at once, utility companies must prioritize repairs across large geographic areas.

As a result, homeowners living well inland may experience prolonged outages despite being far from the coast.

Which Inland Homes Are Most Vulnerable to Hurricanes?

While nearly any home can lose power during a hurricane, some properties face greater risk than others.

Homes surrounded by mature trees are more vulnerable to fallen limbs damaging power lines. Rural properties often rely on above-ground electrical infrastructure that can be more susceptible to wind damage. Homes with private wells may lose access to running water if electricity is interrupted, while families who depend on refrigerated medications or electrically powered medical equipment may face additional challenges during extended outages.

Even suburban neighborhoods with underground utilities can experience outages if nearby substations or transmission equipment are damaged. Understanding your home's unique vulnerabilities can help you prepare before hurricane season begins.

What Does NOAA Recommend for Inland Hurricanes?

NOAA encourages homeowners to prepare before hurricane season, regardless of where they live. Storm tracks can change quickly, and inland communities often experience flooding, tornadoes, and damaging winds long after hurricanes make landfall.

Preparation should include:

  • Monitoring trusted weather forecasts

  • Reviewing your family's emergency plan

  • Stocking emergency food and water

  • Charging phones and backup battery packs

  • Securing outdoor furniture and equipment

  • Reviewing your backup power options

Preparing early helps avoid the last-minute rush for supplies and allows homeowners to address maintenance or repairs before severe weather threatens.

How Can Emergency Standby Generators Help in Inland Hurricanes?

Many homeowners associate backup generators with coastal living, but inland power outages can be just as disruptive.

An emergency standby generator provides automatic backup power whenever utility service is interrupted. Unlike portable generators, standby generators are permanently installed outside the home and connected directly to the electrical system and fuel supply.

When an outage occurs, an automatic transfer switch detects the loss of utility power, starts the generator, and restores electricity within seconds. This way, homeowners don't need to go outside during severe weather to manually start any equipment or connect extension cords.

Benefits During Inland Hurricanes

Reliable backup power helps homeowners continue operating many of the systems they rely on every day, including:

  • Heating and cooling equipment

  • Refrigerators and freezers

  • Well pumps

  • Internet and communication devices

  • Security systems

  • Medical equipment

  • Lighting

Maintaining power also helps families stay connected, preserve food and medications, and remain more comfortable while utility crews work to restore service.

Because standby generators operate automatically, homeowners can focus on keeping their families safe instead of worrying about setting up backup equipment during dangerous weather.

The Bottom Line: Should Inland Homeowners Invest in Backup Power?

Whether you live on the coast or several hundred miles inland, hurricanes can interrupt daily life long after making landfall. While inland communities may not experience storm surge, they often face many of the same challenges, including fallen trees, flooded roads, damaged electrical infrastructure, and extended power outages.

For homeowners who rely on electricity for heating and cooling, refrigeration, medical equipment, well pumps, internet service, or home security, an emergency standby generator provides dependable backup power when it's needed most.

Preparing before hurricane season allows homeowners to evaluate their home's risks, complete routine generator maintenance, and ensure essential systems remain protected if the electrical grid goes down. For many inland homeowners, investing in backup power centers around protecting homes, families, and peace of mind. Find a KOHLER Home Generators dealer near you today.

FAQs

What is an inland hurricane?

An inland hurricane refers to the impacts a tropical storm or hurricane continues to cause after moving away from the coastline. While severe storms gradually weaken after landfall, they often still produce damaging winds, flash flooding, tornadoes, and extended power outages hundreds of miles from the coast.

Can a hurricane still cause power outages after it weakens?

Yes. Even storms that weaken after landfall can interrupt electrical service for days. Heavy rainfall softens the ground, making trees easier to uproot in strong winds, and fallen trees are a leading cause of downed power lines during tropical systems.

Do inland homes really need backup generators?

Many homeowners assume generators are only necessary for coastal properties. Still, inland communities often end up with fallen trees, flooding, and damaged electrical infrastructure that can cause outages lasting several days, regardless of distance from the coast.

Which homes are most vulnerable to power outages during a hurricane?

Homes that are surrounded by mature trees, rural properties with above-ground power lines, and houses that have private wells or medical equipment face greater risk. Even suburban homes with underground utilities can lose power if nearby substations are damaged.

What does NOAA recommend for hurricane preparedness?

NOAA recommends that all homeowners, coastal and inland, monitor weather forecasts, review emergency plans, stock food and water, charge devices and battery packs, secure outdoor equipment, and review backup power options before hurricane season begins.

How fast does a standby generator restore power during a storm?

An automatic transfer switch detects the loss of utility power and starts the generator, restoring electricity within seconds. Homeowners don't need to go outside during severe weather to start equipment manually.

KOHLER Generators Logo

© 2026 Discovery Energy, LLC dba Rehlko. All Rights Reserved