How Long Does a Home Generator Last?
TLDR
Most home standby generators can run continuously for several days during an outage, and can last 15 to 30 years with proper care.
Runtime depends on fuel supply and load, while lifespan depends on maintenance, usage, and installation quality.
Generators connected to a natural gas line can run continuously throughout an entire outage, while propane systems depend on tank size.
Routine servicing, like oil changes and inspections, is the main factor in getting the most years out of your generator system.
Key Takeaways:
Generators can usually run continuously for several days during an outage, and most home generators last 15-30 years with proper care.
Generator runtime depends on fuel supply and load, and maintenance plays a key role in overall generator lifespan.
Long-lasting generators, like those from KOHLER Home Generators, provide reliable backup power.
How long can a generator run and last? Most home standby generators can run for several days continuously during an outage, and they typically last 15 to 30 years as long as you take care of proper maintenance and servicing as needed.
Generator lifespan and runtime are two different factors. Runtime refers to how long the generator can operate during a single outage, while lifespan refers to how many years the system will function reliably.
How Long Can a Generator Run?
Standby generators are designed for extended operation. When connected to a natural gas line, they can run continuously throughout an outage. Propane-powered systems can also run for days, depending on tank size and fuel availability.
How Long Do Generators Last?
With proper care, most home generators can last between 15 and 30 years. Your generator’s lifespan depends on how often the generator runs, how well it’s maintained, and the environment it operates in. Regular servicing, including oil changes and inspections, can help extend the life of your generator system.
Several factors influence how long a generator lasts:
Maintenance: Routine service keeps your generator system running efficiently
Usage: Frequent or extended outages increase wear on your generator
Installation quality: Proper generator setup helps prevent long-term issues
Environmental conditions: Extreme weather can impact generator components over time
A reliable generator provides long-term protection during outages. Systems that are properly maintained can deliver consistent performance for years, helping you avoid disruptions and protect essential systems during an outage. Find a KOHLER Home Generators dealer near you to secure your backup power and stay ahead of outages for years to come.