Skip to main content
1-844-731-7989
KOHLER Generators Logo

Search

How do standby generators add value to your home?

TLDR

  • Standby generators can increase home value by roughly 3% to 5%, making them a practical long-term investment.

  • Buyers are increasingly drawn to homes with built-in backup power, especially in storm-prone areas.

  • A standby generator keeps essential systems like HVAC, refrigeration, and security running during outages.

  • A standby generator automatically restores power within seconds, giving homeowners lasting comfort and reliability.

Key Takeaways:

  • Standby generators can increase home value by improving buyer appeal, as backup power is a very desirable feature in outage-prone areas.

  • Generators help protect essential home systems and can support long-term investment and resale value.

  • Automatic power restoration adds convenience and reliability for homeowners.

Does a home standby generator increase home value? Yes, standby generators can increase a home’s value by improving reliability and protecting essential systems during power outages.

Homebuyers are now placing more importance on features that provide comfort, safety, and convenience. In areas that are especially prone to storms or extreme weather and grid issues, backup power is typically seen as a desirable upgrade. A home that has a standby generator offers an extra level of reassurance that key systems will continue operating, even in the event of an outage.

Increased Buyer Appeal

A standby generator can make a property stand out in a competitive market. Buyers might be more likely to choose a home with built-in backup power, especially if they work remotely, regularly rely on medical devices, or just want to avoid disruptions during storms. The added convenience of a generator can make a home that much more appealing.

Protection for Essential Systems

Power outages can interrupt systems like heating and cooling, refrigeration, sump pumps, and home security. A standby generator helps maintain these systems, reducing the risk of damage and costly repairs while also keeping you comfortable and offering peace of mind.

Long-Term Investment Value

A professionally installed standby generator can increase a home’s value by approximately 3% to 5%. While the exact increase in home value can vary based on location, many homeowners see a standby generator as a long-term investment. A standby generator can support higher resale appeal and offer ongoing benefits by maintaining comfort and reducing downtime during outages.

A permanently installed standby generator can automatically restore power within seconds, helping your home remain functional when utility power is unavailable. Find a KOHLER Home Generators dealer near you to get your standby generator installed.

KOHLER Generators Logo

© 2026 Discovery Energy, LLC dba Rehlko. All Rights Reserved

How do standby generators add value to your home? | KOHLER Generators