Skip to main content
1-844-731-7989
KOHLER Generators Logo

Search

Can You Run a Generator in the Rain?

TLDR

  • Portable generators and rain don't mix because water exposure risks electrical shock, short circuits, and equipment damage.

  • If you have to run a generator in wet weather, keep it dry, elevated, ventilated, and always outdoors.

  • Portable generators need protection from rain, but standby generators are built to run safely through storms without any manual setup.

  • Rain turns generator use into a safety hazard, and the right enclosure, placement, and generator type make all the difference.

Key Takeaways:

  • Do not operate portable generators in direct rain without proper protection, as water exposure increases the risk of electrical shock and damage.

  • Use weather-safe generator covers and keep your generator dry and ventilated.

  • Do not operate your generator indoors, as this poses carbon monoxide risks.

  • For a safer option, standby generators are designed for safer outdoor operation.

Can you run a generator in the rain? Generally, portable generators should not be operated in direct rain or wet conditions unless properly protected, and this is because water exposure can create serious electrical hazards. Permanently installed standby generators, however, are actually designed for outdoor installation and can operate safely during storms when installed and used correctly.

Generators produce electricity, and combining electrical equipment with water increases the risk of shock, device damage, or even fire. Operating your generator in the rain without protection can create unsafe conditions for both your equipment and anyone nearby.

Why Is Running a Generator in the Rain Dangerous?

Water can enter electrical components in your generator, increasing the risk of short circuits and electrical shock. Wet conditions can also damage the generator's internal components, leading to performance issues or system failure in the future. For portable generators, exposure to rain is especially risky because these devices are not designed to be waterproof.

How Can You Use a Generator Safely in Wet Weather?

If you need to run a generator during rain, take these precautions:

  • Place the generator in a dry, well-ventilated area outdoors

  • Use a generator-rated cover or enclosure designed to keep rain out while allowing airflow

  • Never operate a generator indoors, in garages, or near windows due to carbon monoxide risks

  • Keep your generator elevated and away from standing water

Permanently installed standby generators like those from KOHLER are designed for outdoor use and are built for permanent outdoor installation. They’re engineered to operate in a range of weather conditions, including rain and storms. Because these systems are enclosed and automatically turn on during outages, they offer safer operation during storms when installed correctly.

A standby generator can automatically restore power within seconds, helping your essential systems continue running without requiring any manual setup in dangerous conditions. Find a KOHLER Home Generators dealer near you to get your backup power installed.

KOHLER Generators Logo

© 2026 Discovery Energy, LLC dba Rehlko. All Rights Reserved