1-844-731-7989
KOHLER Generators Logo

Search

A KOHLER generator sitting in the yard of a stone house in a dark scenario illuminated by lightsGenerators 101

What to Know Before Buying a Generator

Key Takeaways:

  • Automatic Backup Power: KOHLER standby generators keep your home powered during winter outages—no manual startup needed.

  • Stay Safe & Warm: Maintain heating, lighting, and critical appliances even in severe snowstorms.

  • Protect Your Home Systems: Prevent damage to HVAC, sump pumps, and medical devices with reliable power.

  • Winter-Ready Convenience: Installed outside to reduce carbon monoxide risks and operate automatically.

  • Emergency Preparedness: Stay connected, charge devices, and keep your family safe during unpredictable weather.

Never lose power again.

During an outage, your KOHLER ® Generator automatically keeps your power on. So, you and your family can stay safe and connected even in unexpected situations.

What is a Standby Generator?

When the power goes out, a standby generator automatically powers your entire home during an outage, whether you're home or not. The automatic transfer switch (ATS) that is connected immediately signals the generator to start. And once installed, the entire unit operates completely hands-free for you, the homeowner. Talk about peace of mind.

A KOHLER Certified Installer will install the backup generator outside your home, and it will activate automatically within about 10 seconds or less of a power loss. To schedule installation or learn more, contact a KOHLER generator dealer near you for expert guidance and setup.

Whether you're home or away, the automatic transfer switch will engage until the power grid is restored.

You won't need to deal with extension cords or worry about refueling with gasoline or diesel. Your standby generator connects directly to your home's power source, such as natural gas (NG) or liquid propane.

View FAQs

Real Life Stories and Testimonials

Hear from real Kohler Home Generator owners about the difference reliable backup power has made in their lives. Join these satisfied Kohler customers when you request your free quote today.

Elderly couple, walking holding hands through their yard in front of a Kohler home generator.

Power it all

During an outage, your food is the first thing to go. On average homeowners lose about $250 worth of perishable foods without a generator. That’s a lot of hard-earned cash out the window.

Fridge/Freezer

We understand how important it is to keep your electronics running. Feel confident knowing that everything, from medical equipment to chargers, will power on in about 10 seconds. You'll also be able to protect your devices from power surges by holding a consistent voltage level.

Electronics

With uncertain weather, no one can plan for an outage. Feel comfortable knowing your quiet generator will automatically switch on your air conditioning or heat. Beat the heat or stay cool in your home during any weather condition.

Heat/Air Conditioner

Power's off? Keep the lights on!

In less than 10 seconds, watch as your lights power back on, helping you and your family stay safe and comfortable. Having quick access to your lights, you can potentially spot any safety or environmental hazards quickly and efficiently.

Lights

If you use well water, you won't be able to shower or flush the toilet during an outage. No sump pump means you could spend over $26,000 on a flooded basement plus additional repairs on burst pipes or mold removal. Feel confident knowing that you will have secure access to the water you need to continue your day-to-day life.

Water

FAQ


  • We offer a 6kW-150kW range of power. Our experienced dealers will help you choose what you need to keep everything you want powered on.

  • Ideal for backing up your home if there is a black or brown out.

  • Your generator will automatically start and restore power in seconds.

  • Receive power to critical hard-wired systems.

  • No need to worry about refueling. You’ll pick either a natural gas generator (NG) or a liquid propane gas generator (LPG) based on your home.

  • Have high-quality power delivered simultaneously. Our generators won’t harm your electronics.

  • Keep things simple with the help of our dealers who will take care of the installation process for you.

  • Our generators come in over 10 colors, match your generator to fit your style.

EXPLORE HOME GENERATORS

Meet the brains behind your home generator. The ATS is always monitoring your home’s power.

During an outage, it automatically transfers power from the utility to your generator. The ATS restores your home power to the utility grid and turns off your backup power when the main power comes back on.

EXPLORE AUTOMATIC TRANSFER SWITCHES

Zoom in of a modern house with large glass windows, lights inside. There are two people sitting inside the house chatting.

What Size Generator Do I Need?

Estimate your needs and connect with your local certified dealer to get a personalized free quote

Need help with your Kohler home generator?

Call Kohler Home Generator Support: 1-833-393-6650 Hours: Monday – Friday, 8:00am to 4:30pm (CT)

woman answering a call for owner support
KOHLER Generators Logo

© 2026 Discovery Energy, LLC dba Rehlko. All Rights Reserved