Skip to main content
1-844-731-7989
KOHLER Generators Logo

Search

House with its lights on, on a green yard with heavy clouds in the sky.Storm Preparedness

Tornado Season: Powering Through the Storm

Tornado season usually happens from March to June. This is when weather conditions are best for these strong storms to form.

While tornadoes can develop at any time of the day or night, they are most frequently seen in the afternoon hours. Understanding tornadoes can help you to stay informed and prepared during these months when the risk is at its peak.

Ready to protect your house from an outage?

Get a free quote

What is a Tornado? How They Form and Why They Cause Power Outages?

A tornado is a narrow, rotating column of air that extends from a thunderstorm to the ground.

How Does a Tornado Form?

Tornadoes form when warm, humid air near the ground collides with dry, cold air above, creating unstable weather. Strong winds at different heights cause the air to spin horizontally with violently rotating columns of air. If a storm's powerful updraft tilts this spinning air upright, it can turn into a tornado if the funnel cloud touches the ground.

Where Do Tornadoes Form?

Tornadoes happen in many areas of the country. They are most common in the United States, especially in Tornado Alley, which includes Texas, Oklahoma, Kansas, and Nebraska.

How Many Tornadoes occur each year?

About 1,200 tornadoes hit the U.S. yearly. Tornado-related power outages can cause serious damage to homes and communities, which is why many homeowners turn to home generators to maintain power during severe weather events. They disrupt daily life and can lead to big financial losses. When tornadoes damage power lines, transformers, and substations, widespread blackouts can leave households without essential utilities such as heating, cooling, refrigeration, and communication. This can lead to food spoilage, health risks, and costly repairs.

Tornado Preparedness: Why You Need a Standby Generator for Power Outages

Power outages caused by tornadoes can significantly affect residences and businesses, particularly during a tornado watch, warning, or emergency. Recognizing potential outcomes is crucial.

A large brick house with a Kohler generator along a wall in a residential neighborhood at night with a storm and lightning outside and the lights on inside

Tornado Watch vs Warning

Tornado Watch: This means there may be severe storms. It is important to prepare for possible blackouts. Charge your devices and prepare for an outage.

Tornado Warning: Authorities issue a tornado warning when radar reports or detects a tornado. This increases the risk of power failures. High winds and flying debris can damage power lines. Seek shelter.

Tornado Emergency: Officials have declared a tornado outbreak.

Observers have spotted violent tornadoes and tornado strikes, and they expect imminent damage. This often resulting in prolonged outages that disrupt essential services, communication, refrigeration, and day to day operations. Homes may experience food spoilage, health hazards, and HVAC failures.

During tornado season, backup power is crucial for homeowners. It helps them stay safe during power outages caused by tornadoes, especially when solutions are properly selected and installed by a generator dealer near you.

Buying a backup generator, surge protectors, and emergency power solutions keeps homes safe, comfortable, and connected during bad weather.

Get a free quote

KOHLER Generators Logo

© 2026 Discovery Energy, LLC dba Rehlko. All Rights Reserved