Skip to main content
1-844-731-7989
KOHLER Generators Logo
House among trees on a storm with lightnings

Whole House Generator Installation Quote

Backup power for your home with professional installation and local dealer support.

Get Your Free Quote

Call (844) 731-7989 or fill out the form.

Two men preparing a generator instalation

How to get a whole house generator installed

1

Contact us via phone or complete the free quote form

2

We match you with a certified Kohler generator dealer near you

3

Get exact pricing for your home and discuss financing options with a dealer

4

Your dealer installs your backup generator for reliable home power

What is a whole house generator?

A whole house generator automatically powers your home during an outage, keeping essential systems running without interruption.

  • Automatically turns on during power loss

  • Runs on natural gas or liquid propane

  • Provides seamless backup power

  • Protects your home and appliances

Kohler genertor by a white house with leaves
Close of an open KOHLER generator

Comparing Kohler vs. Generac Generators

Kohler and Generac both offer home standby generators—but they differ in performance, durability, and long-term support.

Kohler generators are built for:

  • Consistent power during outages and load changes

  • Heavy-duty construction for long-term reliability

  • Quiet operation for residential use

  • Built-in monitoring and diagnostics

  • Installation and service by certified Kohler dealers nationwide

Real Kohler Generator Owners

Reviews

Casey - Ryegate, MT

★★★★★

“I own a Kohler generator that I bought through Kohler. Having a home generator is definitely a premium. I've had one for 15 years. I have a well water all the time and it is pretty high on my priority list. Having a generator for it makes me the happiest.


Being an electrical contractor, I'm exposed to a lot of different other brands and Kohler is a standout. It's a great product and their quality is really good. They recently changed hands as a corporation so I'm still waiting to see how that works out. Other than that, excellent products and excellent parts availability.”

Reviewed December 7, 2025

Laurie - Houston, TX

★★★★★

"We researched and KOHLER appeared to be the best generator, even though Generac, produces more. It’s of a higher quality. We've used it once since we had it installed in July. We lost power for 20 minutes. It has been seamless. You can't even tell.

And every week we do a test, the generator kicks on for 20 minutes. The time there was an issue, they came out, because we have a warranty. They figured out what the issue was, and they fixed it. We haven't had any problems since. We feel that we are protected. Our pets are safe.

We are safe. It has been a wonderful experience." Reviewed May 4, 2026

Home Generator FAQs


The total cost of a standby home generator depends on several factors, including:

  • Generator size and power capacity

  • Whole-home vs essential-circuit coverage

  • Natural gas or propane setup

  • Electrical and gas line work

  • Permits and site preparation

  • Installation complexity

Because every home is different, most homeowners schedule a free site evaluation to receive a custom recommendation and quote. A certified dealer can assess your home’s power needs and installation requirements before providing pricing.

Most standby generator installations are completed within a few days once equipment and permits are ready. The overall process can take longer depending on:

  • Permit approvals

  • Utility coordination

  • Generator availability

  • Weather and site conditions

  • Gas or electrical upgrades

Yes — financing is commonly available through many authorized dealers.

Yes — a standby generator is specifically designed to start automatically even if you are away from home. When utility power is lost, the generator’s automatic transfer switch (ATS) detects the outage, signals the generator to start, and transfers your home’s electrical load to backup power — typically within about 10 seconds. Once utility power returns, the system automatically switches back and shuts the generator down.

Trusted Name

KOHLER generators are built with a legacy of engineering excellence and are part of the KOHLER® home energy product line, now supported by Rehlko (formerly Kohler Energy). This ensures continued access to the same dependable products, warranty coverage, and nationwide dealer network.

Close up image of a Kohler home generator
Life doesn’t stop when the power goes out.

Here are a few scenarios where a home generator can make all the difference.

Remote workers and home-based businesses can’t afford downtime. Whether you’re on an important video call, managing online orders, or running a storefront, KOHLER generators keep your operations running smoothly—no interruptions, no lost income.

A vacant home is especially vulnerable during a power outage. Prevent costly damage from frozen pipes, mold, or flooding with a reliable generator that automatically kicks in—even when no one is there to turn it on.

For those embracing a self-sufficient lifestyle, a KOHLER generator ensures you have a dependable energy source. Whether you’re living in a remote cabin or an eco-friendly home, you’ll never be left in the dark.

From hurricanes and tornadoes to wildfires and blizzards, extreme weather can knock out power for days—or even weeks. With a KOHLER generator, you can weather the storm with confidence, knowing your home and loved ones are protected.

Whether it's a wine collection, musical instruments, exotic pets, or more, KOHLER keeps your home climate stable and your valuables safe. Safeguard what matters most.

Talk to a real person

Call 844-844-1732 to speak with a helpful Kohler professional. Hours of operation: Mon-Fri 7AM-7PM CST

KOHLER Generators Logo

© 2026 Discovery Energy, LLC dba Rehlko. All Rights Reserved